How to make "mfg uboot" and "mfg uImage" using Yocto ?
Cheers, Jaakko
From "Freescale Yocto Project User's Guide" :
"A manufacturing tool kernel is built by using the imx_v7_mfg_defconfig,
while the default kernel is built by using the imx_v7_defconfig."
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hey thanks!
I use
./oe bb sdr-linux-image
to build the kernel image.
So how I should modify it for the MFG ?
BTW, is it true that for MFG support for Yocto, you need the 3.10.x kernel ?
I have to use 3.0.35 in my project.
Hello,
Please refer to section 3.9 (Building Manufacturing Firmware) of
"i.MX_6Dual6Quad_SABRE-SD_Linux_User's_Guide.pdf" regarding
MFG configuration.
Regards,
Yuri.
Use following commands
bitbake u-boot-imx to generate u-boot.
bitbake linux-imx to generate uImage.
Thanks
Saurabh