Code:
XREF __SEG_START_PhoneNumbers XDEF test, def_phone1 PhoneNumbers: SECTION;Factory default phone numbers def_phone1 dc 0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0def_phone2 dc 0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0def_phone3 dc 0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0def_phone4 dc 0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0def_phone5 dc 0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0def_pin dc '000000',0,0,0,0,0,0,0,0,0,0def_start_msg dc 'Watchguard Alarms ',0MyCode: SECTIONtest: ldhx __SEG_START_PhoneNumbers
make sure to either use one of the labels in section PhoneNumbers or to disable smart linking for one of them otherwise the linker will not link the section to the application (as it is not used).