Hi,
I meet some problems while trying to reset/reboot our ls1021a board.
If I issue the reboot command, our board will halt and promt
mxc_restart: Watchdog reset failed to assert reset
The same thing happens in u-boot too. I have no ideas about it.
I have checked those WDOG1 registers and they are the same as values on TWR board.
Can anyone help me or give me any advice?
Thanks.
Hello H Wei,
In the software, Watchdog reset is generated by writing Software Reset Signal(SRS) bit of the Watchog Control Register(WDOG_WCR) to assert wdog_rst signal.
For details please refer to the section "40.3.3.1 Watchdog reset generation" in LS1021ARM reference manual, please check to "wdog_rst_b" and "HRESET" signals referring to the timing diagram.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yiping,
If I set SRS bit to 0, the TWR board will reboot, but it doesn't work on our board.
I'll try to find out the reason.
Thanks