We have a 200K design running in a single chips 5213.We need to implement new features wich will not fit into 256K.What is the next Freescale solution for this design?We have a strong cost competition problem.At a glance a V2 512K single chip would be the very best for it.I took a look into external memory devices, but the cost envolved in power and memories arrangement are too high for this design.The design is entirely based on CodeWarrior 6.4, wich we would like to keep.
Thanks
Ricardo Raupp
Features | MCF5213 | MCF5216 |
Freq. (MHz) | 66, 80 | 66 |
MIPS (Dhrystine 2.1) | 76 | 63 |
Flash (KB) | 256 | 512 |
SRAM (KB) | 32 | 64 |
Memory Controller | - | SDR SDRAM |
CAN | 1 | 1 |