Hello, I am using cw10.4, built a project with k12dx256vlh5, now at the end of the project and the release option as to debug is not available, has that been discontinued or I have to do something else to go into the release version. This is supposed to free up the Jtag debug port. I do not use the debug port for other functions. interested in knowing about release.
Thanks,
jeevan
Hello Jeevan.
Let's see Debug and Release in the Desktop World:
In the Desktop World, ‘Debug’ and ‘Release’ builds have following typical meaning:
By default, debug and release mode is the same in CW10. in a MQX project, the difference between debug mode and release mode is optimization level setting.
In debug mode: optimization level is 1.
In release mode: optimization level is 4.
You can also refer Erich blog for this topic
http://mcuoneclipse.com/2012/06/01/debug-vs-release/
=====================================================================
if this answers your question, please click on "Correct Answer" button,. thansk!
Best Regards,
Zhang Jun