Hello,
i have a problem when building my rootfs in buildroot 2014.05.
when buildroot is downloading the packages the files have the size of 0bytes. so i think they were not downloaded.
my mirror is :
FREESCALE_IMX_VERSION = 3.5.7-1.0.0
FREESCALE_IMX_SITE = http://www.freescale.com/lgfiles/NMG/MAD/YOCTO/
or
FREESCALE_IMX_VERSION = 3.0.35-4.0.0
# No official download site from freescale, just this mirror
FREESCALE_IMX_MIRROR_SITE = http://download.ossystems.com.br/bsp/freescale/source
is there another mirror where I can download the files with buildroot? i can search for the files and i already have some of them but this is no solution because the mirrors have to be right when customers want to build buildroot ...
regards andi
Unfortunately these mirror does not seem to be part of the official Community BSP. Maybe some user which used these files can tell us if they were replaced.
Perhaps the following document might help: