No video subtitles on imx6 with gstreamer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No video subtitles on imx6 with gstreamer

1,657 Views
jordan38
Contributor II

Hi community,

I am trying to display subtitles on a imx6 solo based board with gstreamer0.10

The setup is the following:

rootfs built with yocto master-next, image based on fsl-image-multimedia, and MACHINE is imx6solosabresd.conf, linux kernel is 3.10.31 BETA.

I have a video file which contain 6 tracks : 1 video, 3 audio and 2 subtitles which I am streaming in multicast with this command : cvlc --repeat videoHD.raw --sout '#udp{dst=239.255.42.1:1234}' --sout-all --sout-keep

ScreenshotVLC.png

I am using the following gstreamer command line to display video and subtitles without audio for the moment:

gst-launch udpsrc multicast-group=239.255.42.1 port=1234 caps='video/mpegts, systemstream=(boolean)true, packetsize=(int)188'  ! aiurdemux name=demux demux. ! queue ! h264parse ! vpudec low-latency=true ! dvbsuboverlay name=overlay ! imxv4l2sink demux. ! "subpicture/x-dvb" ! queue ! overlay.

In results, I have the following traces and nothing on the HDMI out:

MFW_GST_V4LSINK_PLUGIN 4.0.1 build on Sep 19 2014 16:09:46.
Setting pipeline to PAUSED ...
[INFO]    Product Info: i.MX6Q/D/S
vpudec versions :smileyhappy:
    plugin: 4.0.1
    wrapper: 1.0.54(VPUWRAPPER_ARM_LINUX Build on Sep 19 2014 16:08:56)
    vpulib: 5.4.26
    firmware: 3.1.1.46060
Pipeline is live and does not need PREROLL ...
Setting pipeline to PLAYING ...
Aiur: 4.0.1
Core: BLN_MAD-MMLAYER_MPG2PARSER_04.04.23  build on Apr 11 2014 07:20:12
  mime: video/mpeg, mpegversion=(int)[1,2]; video/mpegts, systemstream=true; video/x-cdxa
  file: /usr/lib/imx-mm/parser/lib_mpg2_parser_arm11_elinux.so.3.1
New clock: GstSystemClock
Content Info:
    Seekable  : No
    Size(byte): -1

Mpeg2CreateParser:parser created successfully
Movie Info:
    Seekable  : No
    Live      : Yes
    Duration  : 0:00:00.000000000
    ReadMode  : File
    programs    : 1
    Track     : 4

Track 00 [audio_001045] Enabled
    ppid: 1, ppid 69
    Duration: 0:00:00.000000000
    Language: qaa
    Mime:
          audio/eac3, channels=(int)6, rate=(int)48000, bitrate=(int)999
Track 01 [audio_001046] Enabled
    ppid: 1, ppid 70
    Duration: 0:00:00.000000000
    Language: ???
    Mime:
          audio/eac3, channels=(int)6, rate=(int)48000, bitrate=(int)999
Track 02 [audio_001044] Enabled
    ppid: 1, ppid 68
    Duration: 0:00:00.000000000
    Language: ???
    Mime:
          audio/eac3, channels=(int)6, rate=(int)48000, bitrate=(int)999
Track 03 [video_001048] Enabled
    ppid: 1, ppid 72
    Duration: 0:00:00.000000000
    Language: und
    Mime:
          video/x-h264, parsed=(boolean)true, alignment=(string)au, stream-format=(string)
          byte-stream, width=(int)1920, height=(int)1088, framerate=(fraction)30/1
[INFO]    bitstreamMode 1, chromaInterleave 0, mapType 0, tiled2LinearEnable 0
[WARN]    VPU iram is less than needed, some parts don't use iram
set v4l rotate sucessfully
>>V4L_SINK: Actually buffer status:
    hardware buffer : 12
    software buffer : 0
full screen size:1920x1080
[V4L Update Display]: left=0, top=0, width=1920, height=1080
set v4l display crop sucessfully

(gst-launch-0.10:731): GStreamer-CRITICAL **: gst_buffer_create_sub: assertion 'buffer->mini_object.refcount > 0' failed

(gst-launch-0.10:731): GStreamer-CRITICAL **: gst_mini_object_unref: assertion 'mini_object->refcount > 0' failed

** (gst-launch-0.10:731): CRITICAL **: gst_base_parse_push_frame: assertion 'frame->buffer != NULL' failed

I note that the demuxer "aiurdemux" don't see subtitles tracks.

What can cause this kind of problems?

regards,

Jordan

6 Replies

920 Views
jordan38
Contributor II

Hi,

Someone could help me please, I don't understand why "aiurdemux" don't demux DVB subtitles included in the file?

regards,

Jordan

0 Kudos

920 Views
joanxie
NXP TechSupport
NXP TechSupport

Currently only support text based external .srt file as subtitle, also the .srt file is UTF-8 coded. if you need to use build-in subtitle, we will release in the next version.

0 Kudos

920 Views
jordan38
Contributor II

Hi,

Thank you for your response.

When will you release the next version?

regards,

Jordan

0 Kudos

920 Views
joanxie
NXP TechSupport
NXP TechSupport

currently I don't have specific data

0 Kudos

920 Views
jordan38
Contributor II

Hi,

Do you have news informations about next release of gstreamer0.10 or "aiurdemux" plugin to support build-in subtitle?


regards,

Jordan

920 Views
benhenricksen
Contributor III

Any update on this support for built in sub-titles?

0 Kudos