IMX6Q PAL video output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q PAL video output

595 Views
sharathm
Contributor II

Hi,

I am facing a problem with video output from IMX6q sabrelite board.

I am feeding a video input through CSI0 of IPU0 as per the image attached below

tv-in.jpg

But the output is as below from the HDMI interface

HDMI output.jpg

can anyone please suggest me whats wrong with the configuration or what might be the issue.

Thanks in advance.

Labels (3)
0 Kudos
3 Replies

487 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sharath

for sabrelite board one needs to use BSPs built for that board, please look at

http://boundarydevices.com/tag/camera/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

487 Views
sharathm
Contributor II

Hi igorpadykov

I am using L3.0.35_4.1.0_ER_SOURCE_BSP

with linux 10.04 LTS which is, i think the board support package for imx6 sabrelite board.

0 Kudos

487 Views
igorpadykov
NXP Employee
NXP Employee

This BSP is written and tested for freescale reference boards,

not sure that it supports sabrelite, though you can find sources there.

Board maintainer.jpg

To be sure I would suggest to post that on

meta-fsl-arm mailing list, so maintainers for this board

could try to assist you

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

igor

0 Kudos