I'm using the MPXV5004G pressure sensor. I wish to record
sensitive changes in my breathing. I hooked it up to a
10-bit analog to digital converter and typical breathing is
moving the output value maybe 1 point at best.
I wish to amplify the sensitivity, but I notice that the
MPXV5004G has error of 1.5% or 2.5%. This seems to say
that the output value error is greater than 1 point out of
1024 values, so even if I amplified the changes, could I
trust them?