We have a permanent floating license to CW 10.2. I would like to upgrade the MQX version I am using for a project from 4.0.2 to 4.1.1 . The problem is that 4.1.1 uses the new GCC compiler. Is there any way I can still compile the new MQX versions with CodeWarrior 10.2? Is there some way to install support for the GCC toolchain in CW 10.2?
Hi,
I don't remember if the GCC was or not included in the MCU v10.2.
- I will re-install it -
Under MCU V10.6, the GCC is delivered under the installation folder \CW MCU v10.6\Cross_Tools\arm-none-eabi-gcc-4_7_3.
Can you use the GCC under MCU V10.2 ?
I think yes ... you can call the tool in command line (we're using this way to build project).
Now building the MQX lib, it's another story.
I think it will not be easy ...
I don't recommend you this configuration.
Have a great day,
Pascal Irrle
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------