I use Kinetis Design studio 1.1.0 with Processor expert, (uc MK64F),
I want to create a DSPI : first i create a component DMA (component library -> kinetis SDK -> peripheral driver -> DMA -> fsl_DMA) then i try to create a component DSPI (component library -> kinetis SDK -> peripheral driver -> communication -> fsl_DSPI) but the following message appear :
" Error during adding referenced component/template "fsl_dspi_edma".
Component is either missing or corrupted. "
Can you help me ?
Solved! Go to Solution.
Hello Pe Tapie,
I have reproduce the problem on Linux Ubuntu 14.04 32-bit (there is problem with a path). Processor Expert team has prepared a hot fix, see the attached package.
Please, copy the content of the package into you installation, see detailed instruciton in release notes (hot_fix_KDS_1_1_0_PEXMCU-288.txt) in the hot fix package.
Hello Pe Tapie,
You can refer to the document C:\Freescale\KSDK_1.0.0\doc\Kinetis SDK K64 User's Guide.pdf, chapter “4.4 Kinetis Design Studio IDE”, that comes in the installation files of SDK. It explains the steps that need to be followed to fix the environment variable and apply an update to Kinetis Design Studio, after following these steps create a new project and try to add the fsl_DSPI component to your project. If you still get the same error please upload a screenshot of it.
In case you haven’t installed Kinetis SDK here is the link where you can download it: http://www.freescale.com/KSDK
Regards!
Carlos
Hello Carlos,
Thanks for your answer but I have already instal the update for Kinetis Design Studio, so the problem still occur.
I work on Ubuntu 12.04 and I use MQX KSDK
When I want to add the fsl_DSPI to my project the following message apear :
And when I go in Properties of the component :
Thanks for your help,
Hello Pe Tapie,
I have reproduce the problem on Linux Ubuntu 14.04 32-bit (there is problem with a path). Processor Expert team has prepared a hot fix, see the attached package.
Please, copy the content of the package into you installation, see detailed instruciton in release notes (hot_fix_KDS_1_1_0_PEXMCU-288.txt) in the hot fix package.
Hello Marek,
Thanks for your answer, the directions you gave me allowed me to solve the problem.
Hi PE,
I refer to your screenshot make a try , there is no errors. and you can add the component "fsl_edma" through fsl_edma -> new component ( in the screenshot ) .
Hope it helps
Alice