p2020 nor flash s29gl256p erase failed, blank check failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

p2020 nor flash s29gl256p erase failed, blank check failed

1,124 Views
tianli1
Contributor II

we designed a board with P2020 processor!

the nor flash is s29GL256p, we cann't flash into it a bin file ,we can even not erase the chip:

we use codewarrior 10.3. in the flash programmer,we select  erase whole device. it completed with errors!

the print is as follows:

fl::target -lc "LC for Simple Flash"

fl::target -b 0x2000 0x30000

fl::target -v off -l off

cmdwin::fl::device -d "S29GL256P" -o "16Mx16x1" -a 0xfe000000 0xffffffff

cmdwin::fl::erase all

Beginning Operation ...   

-------------------------

Performing target initialization ...   

Downloading Flash Device Driver ...  

Reading flash ID ...

Erasing entire flash ...   

Erasing ...

Erase Command Succeeded   

cmdwin::fl::blankcheck all

-------------------------

Downloading Flash Utility Driver ...  

Performing Blank Check from 0xFE000000 to 0xFFFFFFFF ...   

Blank Checking ...

Error:  Blank Check failed.

Error: Blank Check failed.

by the way we use CPLD to latch the multiplexd LAD0~~LAD15 address to Nor.

0 Kudos
Reply
1 Reply

620 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Li Tian,

Probably problem exists in DDR controller configuration, please enable "Verify Target Memory Writes" in PA Flash Programmer Task panel, if the memory type error is encountered, please try to use SRAM initialization file in Freescale\CW PA v10.3\PA\PA_Support\Initialization_Files\QorIQ_P2.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply