Hi All,
We want to boot IMX6 device from eMMC interface (SD3)
so we need to configure the boot device type by BOOT_CFG[7:4] eFUSEs as 0110 configuration
i.MX 6Dual/6Quad Applications Processor Reference Manual
From Table 5-4
we should setting 0x450
imxotp blow --force 5 0x00005060
and if we need WDOG support
we should setting 0x460
imxotp blow --force 6 0x00200000
Is it correct or not?
Hi tsai
it is unclear which BOOT_CFG you are trying to blow.
Please use Table 5-7 SD/eSD Boot Fusemap IMX6DQRM
and below links
Q&A: How to program i.MX6 eFUSE?
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello igor
thanks for your reply.
I'm sorry I did not describe clearly.
My board is based on eMMC sdhc3
I have already boot from setting Boot Mode[1:0]= 10 (Boot from Board setting)
and gpio setting BOOT_CFG1[7:4] =0110 , BOOT_CFG[6:3] = 1010
then i want to test setting Boot Mode[1:0]= 00 (Boot from fuse)
I think setting should be
0x450[31:0] = 0x00005060
and i try to add WDOG for serial download
0x460[31:0] = 0x00200000
or i should setting 0x460[31:0] = 0x00200010 ?
thanks for your help
Hi tsai
could you explain your choice with meaning every fuse bit per bit from this table?
I can understand :
"WDOG for serial download
0x460[31:0] = 0x00200000"
and think that this is right.
~igor
Hello igor,
I have set up 0x450[31:0] = 0x5060, 0x460[31:0]=0x200010
use
echo 0x5060 > /sys/fsl_otp/HW_OCOTP_CFG4
echo 0x200010 > /sys/fsl_otp/HW_OCOTP_CFG5
and all work fine
thanks for your help
Thank you, very helpfullll.