Rotation of I.MX53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Rotation of I.MX53

660 Views
chengwu
Contributor I

Hi all,

I'm developing a WinCE7 BSP on an i.MX53 board, and my BSP is based on the i.MX53 SMD BSP, I have a TFTLCD on my board, and the resolution is 240*320, now I need to rotate the display, and I want to use the IRT unit of IPU to do this, I think use IRT unit will be faster and could get better performance, could anybody tell me how can I do this?

Thank you very much.

Labels (3)
0 Kudos
Reply
1 Reply

545 Views
igorpadykov
NXP Employee
NXP Employee

Hi cheng

please check sect.11.4.2.4 Using The Display Driver Control Panel Application,

sect.11.4.3.1 Rotation Support, WCE700_MX53_ER_1105_SMD_ReferenceManual.pdf

IMX53_TABLET_1105_WCE7_BSP_DOCS

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply