I've noticed that when using the Memory View window, it doesn't always tell the truth. Most of the time I can examine memory regions or CPU registers, but occasionally there are locations that just show up as all FF. I know they aren't, because I can put *(address) in the expression window, and it tells me what I expect to see. For example, if I look at SRAM between 0x1FFFF000 and 0x1FFFF040 on a KE06, it shows 0xFF for all those locations.
Hi David,
On my FRDM-K64F board with P&E Multilink interface I've reproduced the problem too.
The problem occurs occasionally.
I've executed with the same project the same process several time:
- clean,
- build,
- launch debug,
- show memory at Memory Browser and Memory component,
- run the debugger (bkpt is set),
- stop on bkpt,
- show Memory Browser and Memory component.
Half of the time the Memory displays right value.
Please have a look jpgs attached.
Is it same issue ?
Have a great day,
Pascal Irrle
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Pascal, yes, that's the kind of thing I'm seeing. I can set the expression window to show the contents of a location, and it will show one thing, but the memory view window may show all FF.
Hi David,
Thanks for info.
I will log the problem in our bug base.
Development team will investigate the problem.
Have a great day,
Pascal Irrle
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------