Dear,
I am trying to setup a custom display on a IMX6SLEVK and I am facing some problems.
In my board is equipped with a 240x320 resolution LCD. I want to modify the kernel of the resolution to 320x240 IMX6SLEVK. If you do need to resolve this issue, modify the kernel somewhere?
Best regards,
Chu
Hi chu yeonsoo,
Which BSP are you using?
Have a great day
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear, Dan
BSP is being developed fsl-community-bsp-platform (daisy: branch). Also developed in the Yocto project.
In addition, I use the ili9341 lcd controller in our platform.
Have a nice day
Chu