Dear sir/madam,
We are using imx6Q sabresd platform for our development with Linux
3.10.17_1.0.0-GA BSP.
In above link shows that, the anatop "reg_pu" value is set to 0x1F which
is linux-3.0.35 kernel.
@@ -81,6 +101,21 @@ void mx6_cpu_regulator_init(void)
regulator_set_voltage(cpu_regulator,
cpu_op_tbl[0].cpu_voltage,
cpu_op_tbl[0].cpu_voltage);
+ if (enable_ldo_mode == LDO_MODE_BYPASSED) {
+ /*digital bypass VDDPU/VDDSOC/VDDARM*/
+ reg = __raw_readl(ANADIG_REG_CORE);
+ reg &= ~BM_ANADIG_REG_CORE_REG0_TRG;
+ reg |= BF_ANADIG_REG_CORE_REG0_TRG(0x1f);
+ reg &= ~BM_ANADIG_REG_CORE_REG1_TRG;
+ reg |= BF_ANADIG_REG_CORE_REG1_TRG(0x1f);
+ reg &= ~BM_ANADIG_REG_CORE_REG2_TRG;
+ reg |= BF_ANADIG_REG_CORE_REG2_TRG(0x1f);
+ __raw_writel(reg, ANADIG_REG_CORE);
+ /* Mask the ANATOP brown out interrupt in the GPC. */
+ reg = __raw_readl(gpc_base + 0x14);
+ reg |= 0x80000000;
+ __raw_writel(reg, gpc_base + 0x14);
+ }
clk_set_rate(cpu_clk, cpu_op_tbl[0].cpu_rate);
But with reference of Linux 3.10.17_1.0.0-GA BSP, During the LDO bypass
the "reg_pu" value is not set to 0x1F as mentioned below. Please clarify.
file:u-boot-imx/arch/arm/cpu/armv7/mx6/soc.c
void set_anatop_bypass(void)
{
struct anatop_regs *anatop = (struct anatop_regs *)ANATOP_BASE_ADDR;
u32 reg = readl(&anatop->reg_core);
/* bypass VDDARM/VDDSOC */
reg = reg | (0x1F << 18) | 0x1F;<-- PMU_REG_CORE's reg_arm & reg_soc
values are set to 0x1F
writel(reg, &anatop->reg_core);
}
Thank you,
Regards,
Ansari
Solved! Go to Solution.
Hi Abdul
1. you can check Chapter 22 Low-level Power Management (PM) Driver
i.MX_6_Linux_Reference_Manual.pdf L3.10.17_1.0.0_LINUX_DOCS
and for example below
2. yes
Best regards
chip
Hi Abdul
yes correct, during the LDO bypass
the "reg_pu" value is not set to 0x1F as given below
file:u-boot-imx/arch/arm/cpu/armv7/mx6/soc.c
because VDDPU is disabled in Uboot :
ENGR00264076-5 i.mx6:shutdown vddpu and pcie phy to save power
LDO bypass code moved to kernel
ENGR00233366-5 Anatop PFUZE: move LDO bypass code to kernel - Gitorious
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Chip,
Thanks for your input on our query.
We understand that the VDDPU will be disabled in the Uboot (to save the power) and it will remains disabled until the kernel the enabling it.
We are using linux-3.10.17 kernel for our development and our device tree is imx6q-sabresd.dtb
The imx6qdl-sabresd.dtsi file having below settings
&gpc {
.........
fsl,ldo-bypass = <1>; /* use ldo-bypass, u-boot will check it and configure */
fsl,wdog-reset = <2>; /* watchdog select of reset source */
pu-supply = <&pu_dummy>; /* ldo-bypass:use pu_dummy if VDDSOC share with VDDPU */
};
we would like to know,
1) In the linux kernel where the VDDPU power anatop register (reg_pu) will be bypassed/enabled?
2) In the case of LDO bypass mode, Is it recommended to bypass (reg_pu value = 0x1F) the VDDPU ?
Thank You,
Regards,
Ansari
Hi Abdul
1. you can check Chapter 22 Low-level Power Management (PM) Driver
i.MX_6_Linux_Reference_Manual.pdf L3.10.17_1.0.0_LINUX_DOCS
and for example below
2. yes
Best regards
chip
hi all,
thanks for help,
i am using 3.10.17 kernel , and the dtsi file as below,
&gpc {
fsl,cpu_pupscr_sw2iso = <0xf>;
fsl,cpu_pupscr_sw = <0xf>;
fsl,cpu_pdnscr_iso2sw = <0x1>;
fsl,cpu_pdnscr_iso = <0x1>;
fsl,ldo-bypass = <1>; /* use ldo-bypass, u-boot will check it and configure */
fsl,wdog-reset = <1>; /* watchdog select of reset source */
pu-supply = <®_pu>; /* ldo-bypass:use pu_dummy if VDDSOC share with VDDPU */
};
the reboot command is not working(not able to restart IMX6), it hangs at "Rebooting... Restarting system."
some times, rebooting but hangs at u-boot when kernel starts "Starting kernel ..."
the reboot feature works with 3.0.35 kernel (same HW) but not in 3.10.17 , i am confused with LDO bypass mode
could you please help me what is missing ?
regards
nagendra
Hi chip,
Thanks for your exact advise.
Thank You,
Regards,
Ansari