Naga
This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.
Thanks,
Yixing
Naga
Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.
Thanks,
Yixing
For more information you can check the datasheet, page 4
http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0100.pdf
Best regards,
Sergio
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Nagaraju,
Yes, F1 version is suitable for LPDDR2. As a recommendation and if it is suitable for your application, you can supply 1.2V with SW3 and 1.8V with SW4.
Best regards.
Jorge.
FSL PMIC PF0100F1 should be suitable, right?