RAppID V2.2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RAppID V2.2.0

3,032 Views
stanleyli
Contributor II

Dose RAppID V2.2.0 support MPC5644A?

I download the RAppid V2.2.0 from freescale website, but it can not work in my computer.

When i tried to execute RAppid, the error window showed the message "E0002--Could not get a licence".

Please give me some tips. Any link or comment would be appreciated.

Labels (1)
0 Kudos
Reply
4 Replies

2,599 Views
miloslavhevjari
Contributor I

Where can I find installer for RAppID V2.2.0 ?

I need support for MPC5554 to by able to run PIL in Simulink with GreenHills (version 5 or 7)

0 Kudos
Reply

2,599 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

2,599 Views
miloslavhevjari
Contributor I

Hi,

the link you provided was broken for long time. Same with the link the RAppID Toolbox v1.2.

The Web team fixed the problem with the links (on request of A. Cecilia Chavez from NXP).

Do you know is there newest MBD Toolbox for MPC5554 supporting R2016b ?

Regards,

-Milo

0 Kudos
Reply

2,599 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

if you check the description, you will see:

"Production Release for of Version 2.2.0.7 of RAppID for the MPC553x, 555x, and 556x Parts."

So, this version does not support MPC5644A.

MPC5644A is supported by:

https://www.freescale.com/webapp/Download?colCode=RAppID_INIT_MPC564xA

But notice that it is commercial software, it is not provided for free. More information can be found here:

RAPPID: RAppID Initialization for Power Architecture

Best Regards,

Lukas

0 Kudos
Reply