Hello Sir,
I want to work with MKL25Z32VFM4(60 pin) controller with Code warrior 10.3.
But when i am trying to create a new BareBoard project with this controller ,options are as
MKL25Z32
MKL25Z64
MKL25Z128
After selecting MKL25Z32 by default MKL25Z32VLK4(80 pin) this controller is getting selected.
Is it possible to select particular MKL25Z32VFM4(60 pin) controller?
i want to select this as there are some pins are not present in MKL25Z32VFM4(60 pin) as compare to MKL25Z32VLK4(80 pin).
I want to generate code for on ADC with MKL25Z32VFM4(60 pin).
There is no VrefH and VrefL pin in MKL25Z32VFM4(60 pin) controller.
But as MKL25Z32VLK4(80 pin) is getting selected i can see the option of reference voltage selection.
How it will select reference voltage forMKL25Z32VFM4(60 pin) controller ?
Regards,
Amreen
Solved! Go to Solution.
Hello,
MCU10.3 is rather old, the most current release is 10.5.
I checked things in MCU 10.5, and I have the VFM4 package available.
You might try this in 10.3:
http://mcuoneclipse.com/2012/08/16/changing-the-cpu-with-processor-expert/
Otherwise, can you try 10.5?
Erich
Hi, Amreen
I think Erich reply is correct. Is it solve your issue? If yes, please mark his reply as correct answer. Thanks.
Best Regards
Paul
Hello,
MCU10.3 is rather old, the most current release is 10.5.
I checked things in MCU 10.5, and I have the VFM4 package available.
You might try this in 10.3:
http://mcuoneclipse.com/2012/08/16/changing-the-cpu-with-processor-expert/
Otherwise, can you try 10.5?
Erich