Hello,
i use Codewarrior 10.5 with a MCF51JU32VFM as controller and a PE-Micro USB multilink flasher (BDM).
I would use the FelxNVM Partition as EEprom and Data storage.
My Config is: 512byte EEPROM usage and 8Kb Data.
FTFL_FCCOB0 = 0x80; FTFL_FCCOB1 = 0x00; FTFL_FCCOB2 = 0x00; FTFL_FCCOB3 = 0x00; FTFL_FCCOB4 = 0x35; //512 bytes eeprom FTFL_FCCOB5 = 0x09; //8kb data partition FTFL_FSTAT |= FTFL_FSTAT_CCIF_MASK; //clear CCIF flag to process eeprom command
This is running, but i need this for debugging, because i place data in the data partiotn during flashing.
When i execute this command (in my program), the data partition is erased. (eeprom is running)
When i try to set the partion during firmware flash or debugging the eeprom function failed. in the attachment is my actual debug settings.
Best Regards,
Sebastian