Hi everyone,
I have implemented code for USB SDcard mass storage device from RAMDISK example provided in MQX 4.0.1. It is working fine on my TWR K60N512 module. Whenever I connect my usb cable between PC and TWR module it will show Removable Disk with its contents. How it is possible to name the device in code so that it will show the device name other than Removable Disk ?
I used the examples of usb RAMDISK and MFS SD card examples to implement this code. Please help me if someone has knowledge on this.
Thanks,
Pramod.
Solved! Go to Solution.
As first I would like note that you cannot access disk simultaneously by PC and MQX.
Only one could have access to disk.
So, there are two possible ways:
As first I would like note that you cannot access disk simultaneously by PC and MQX.
Only one could have access to disk.
So, there are two possible ways:
Thanks Radek S,
I could rename the drive name in second way and its working fine. Is it possible to improve the speed over USB when SD card is mounted as MSD?. I developed this code from usb-msd-device example and my current speed is around 110KB/s. Please help if its possible?
Thanks,
Pramod.