Hello.
I want to check about i.MX6Q.
Do not use the terminal ONOFF in this board.
(It is always ON If the power is supplied.)
There is not a mention of when unused is the terminal ONOFF.
In this case , the terminal ONOFF is correct pull-up ?
Regards,
-okamoto
First, when the TEST_MODE pin is HIGH, it enables an alternate function of ONOFF which is RESET_IN_B.
It is recommended that TEST_MODE should be tied to ground or floated (because it has an internal pull-down).
With TEST_MODE always LOW, the ONOFF button/signal does not pass through as a reset to the i.MX6 SRC.
Next, ONOFF signal has internal (100 KOhm ) pull-up, so can be left floating.
But under noisy environment – if internal 100 KOHm pull up is not strong enough – an external
resistor (of 10 KOhm) may be applied.
Hi, Yuri
Thank you for reply.
TEST_MODE use at the L level.
Because ONOFF pin is not used, I will pull up at 10kohm.
Thank you for information.
Try to consider.
Regards,
-okamoto