ltib "min profile" build ssuccessful.
However, "mfg firmware profile" failed.
The following is error message.
Could anybody let know why???
=================== error message =================
+ [ /home/john/dev/freescale/dev_env/ltib/rpm/BUILD/u-boot-2009.08 != /home/john/dev/freescale/dev_env/ltib/rpm/BUILD/u-boot-2009.08 ]
+ cd /home/john/dev/freescale/dev_env/ltib/rpm/BUILD/u-boot-2009.08
+ [ -n ]
+ make HOSTCC=ccache /usr/bin/gcc -B/usr/bin/ CROSS_COMPILE=arm-none-linux-gnueabi- O=/home/john/dev/freescale/dev_env/ltib/rpm/BUILD/u-boot-2009.08 mx6dl_sabresd_mfg_config
make: *** No rule to make target `mx6dl_sabresd_mfg_config'. Stop.
error: Bad exit status from /home/john/dev/freescale/dev_env/ltib/tmp/rpm-tmp.23807 (%build)
RPM build errors:
Bad exit status from /home/john/dev/freescale/dev_env/ltib/tmp/rpm-tmp.23807 (%build)
Build time for u-boot-v2009.08: 0 seconds
Failed building u-boot-v2009.08
f_buildrpms() returned an error, exiting
traceback:
main:572
Started: Wed Feb 5 15:09:11 2014
Ended: Wed Feb 5 15:09:14 2014
Elapsed: 3 seconds
These packages failed to build:
u-boot-v2009.08
Build Failed
Exiting on error or interrupt
There are my mistakes.