U-boot LTIB option for 'SABRE for Automotive Infotainment Based on the i.MX 6 Series' evaluation board with IMX6U processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

U-boot LTIB option for 'SABRE for Automotive Infotainment Based on the i.MX 6 Series' evaluation board with IMX6U processor

Jump to solution
1,397 Views
stevencao
Contributor I

Hi,

I have a 'SABRE for Automotive Infotainment

Based on the i.MX 6 Series' evaluation board.

My onboard CPU is IMX6U which is i.MX 6DualLite processor.

I was trying to run 'ltib' to build the code.

However,when 'LTIB' presented me the CPU (platform) option, I only could find option for IMX6Q or IMX6S, but NOT IMX6U or IMX6D.

What should I choose?

I was told by Freescale technical support to choose 'IMX6S' and 'IMX6dl_sabreauto' as platform in LTIB menu to build U-boot.

However, in the LTIB configuration menu, for 'Choose your board for U-Boot', there are only two options:
'mx6sl_arm2' and 'mx6sl_evk'.
I could NOT find a 'mx6dl_sabreauto' option.


This morning, I tried 'IMX6Q' processor and did find 'mx6dl_sabreauto' option. Should I choose 'IMX6Q' for IMX6U' processor?


Thanks,


Steven

0 Kudos
Reply
1 Solution
986 Views
Yuri
NXP Employee
NXP Employee

Chapter 3 (Building the Linux Platform) of "i.MX_6Solo6DualLite_SABRE-AI_Linux_User's_Guide.pdf" describes

how to build target system for i.MX 6DualLite.

https://www.freescale.com/webapp/Download?colCode=L3.0.35_4.1.0_LINUX_DOCS&location=null&fpsp=1&Pare...

SABRE for Automotive Infotainment Based on the i.MX 6 Series

View solution in original post

0 Kudos
Reply
3 Replies
987 Views
Yuri
NXP Employee
NXP Employee

Chapter 3 (Building the Linux Platform) of "i.MX_6Solo6DualLite_SABRE-AI_Linux_User's_Guide.pdf" describes

how to build target system for i.MX 6DualLite.

https://www.freescale.com/webapp/Download?colCode=L3.0.35_4.1.0_LINUX_DOCS&location=null&fpsp=1&Pare...

SABRE for Automotive Infotainment Based on the i.MX 6 Series

0 Kudos
Reply
986 Views
stevencao
Contributor I

Would you please send me 'L3.0.35_4.1.0_130816_images_MX6.tar.gz'? I could not find it.


Does this package include all the files, u-boot, uImage and rootfs, which are the same as the ones on evaluation board?


Thanks,


Steven

0 Kudos
Reply
986 Views
SergioSolis
NXP Employee
NXP Employee

You can download it from here:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREPLAT&fpsp=1&tab=Design_Too...

Under: Run-Time Software >> Operating System Software - Board Support Packages >> L3.0.35_4.1.0_DEMO_IMAGE_BSP

And yes, it includes everything you ask for.

0 Kudos
Reply