I used the yocto build to generate images for t4240.
I downloaded the meta-fsl-ppc layer (from: meta-fsl-ppc - Layer containing Freescale PPC hardware support metadata)
and included it into the build and removed the meta-yocto-bsp layer.
The build generated a few images in tmp/deploy/images/t4240qds.
The build was successful, but while I attempted to run using qemu, it failed.
$ runqemu t4240qds
PS: I saw the images folder and I didnt find a .ext3 filesystem, instead I found a rootfs.tar.gz file.
Can I run a t4240 image in qemu?
Thanks in advance.
The SDK Yocto build environment doesn't support runqemu, KVM/qemu virtualization should be implemented on the target board.
fsl-image-flash:meta-fsl-networking/images/fsl-image-flash.bb
fsl-image-core:meta-fsl-networking/images/fsl-image-core.bb
fsl-image-full:meta-fsl-networking/images/fsl-image-full.bb
fsl-image-kvm: meta-fsl-networking/images/fsl-image-kvm.bb
fsl-image-minimal:meta-fsl-networking/images/fsl-image-minimal.bb
fsl-toolchain:meta-fsl-networking/images/fsl-toolchain.bb
The rootfs type can be customized by setting the IMAGE_FSTYPES variable in the
above recipes.
Supported rootfs types include the following:
cpio
cpio.gz cpio.xz
cpio.lzma
cramfs
ext2
ext2.gz
ext2.gz.u-boot
ext2.bz2.u-boot
ext3
ext3.gz.u-boot
ext2.lzma
jffs2
live
squashfs
squashfs-lzma
ubi
tar
tar.gz
tar.bz2
tar.xz