P1022DS DIU interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1022DS DIU interrupt

552 Views
hudi
Contributor II

Dear sir,

     I want to use DIU interrupt,but I do not know the meaning of the Vsync interrupt,the underrun interrupt,and the lines before Vsync interrupt.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

421 Views
yipingwang
NXP TechSupport
NXP TechSupport

For VSYNC and LS_BF_VS interrupts, please refer to the Section 9.5.3 of the P1022 Reference Manual:

If enabled, the VSYNC status bit will always be asserted with the first vsync pulse cycle. With this interrupt, the host can always observe the beginning of a new frame. Beside this, another interrupt, the LS_BF_VS (lines before vsync) can be used to set a deadline for the host to program the pointers for the current next frame. This interrupt is asserted at user-specified lines (set by the LS_BF_VS threshold, Section 9.3.17, “THRESHOLDS Register”) before the vertical front porch (FP_V). The host can program the pointer registers after it detects the LS_BF_VS interrupt.

Figure Figure 9-36 shows a diagram on how these two interrupts can be used to synchronize the host and the DIU.

UNDRUN interrupt.Under run exception interrupt is asserted when display needs data and output buffer filling is lower than or equal to the OUT_BUF_LOW threshold. See please the Section 9.5.5

0 Kudos
Reply