Hi Community,
I have a hardware question.
In my application i want to sample a signal from hall effect sensor in the windows from 0.5V to 4.5V.
To improve the fidelity of the ADC i want to compress the dynamics of the ADC, and put the Vref @ 4.8V. My question is: My connection in the attached document is right? Or a voltage resistor divider is better?
Thanks to everybody in advance for our reply.
Best Regards
You want to lower Vdda, not Vref, right? This would violate ADC Supply voltage Delta to Vdd! See Table A-9.
Hi Edward,
yes! If my calculations are correct my configuration should be good.
As i see in the table A-9 of the datasheet the admited VddA is between 2.7 -5.5V with a Delta to Vdd between -0.1 < Vdd < 0.1V.
The formula to found Delta V is: (VDD-VDDAD)^2 then in my case: (5.00-4.8)^2 = 0.04V that is the admitted range.
What you think?
Thank you!
Diego
(VDD-VDDAD)2 would give (mV)2 units. And you see just millivolts...
Sorry Edward,
i don't understand. if i use the Vdd and VDDAD in mV the result of square elevation is mV^2 ...
Can you give me an example?
Thanks
I replied to your previous message via email. Community engine sometimes faills sending from browser, sometimes from email.
I meant that if delta-Vdda-to-Vdd was calculated as you specified (VDD-VDDAD)^2, then specified limits had to be specified in square millivolts units, not in millivolts. Also there could be no negative limit for this. I don't know exactly what authors of S08DZ datasheet meant, maybe they meant RMS or somethibg, but delta is still specified in mV units.
Ok, I have too many doubts. For safety I put the VDDA to 5V.
Thank you very much for your support Edward!
Best Regards.
Diego