imx6 hdimidogle usb_otg_oc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 hdimidogle usb_otg_oc

Jump to solution
3,876 Views
kingliu
Contributor II

dear all

Refer to the SCH_HDMI_DONGLE_MX6X_REVB2_20130116_1500, the pin of EIM_D21 is used as USB_OTG_OC. MX6Q_PAD_EIM_D21__USBOH3_USBOTG_OC,


And when the status of USB_OTG_OC change , how  the software can detect ?


Is there some register can be read when the USB_OTG_OC is low or high?

Labels (1)
0 Kudos
Reply
1 Solution
2,818 Views
Yuri
NXP Employee
NXP Employee

  USB_OTG_OC signal is intended for overcurrent event from a USB power scheme,

providing VBUS for external device, assuming i.MX6 OTG is in USB host mode. 

OCC and OCA fields of USB PORTSC1 register are affected by USB_OTG_OC signal

state.

View solution in original post

0 Kudos
Reply
2 Replies
2,818 Views
Yuri
NXP Employee
NXP Employee

  USB_OTG_OC signal is intended for overcurrent event from a USB power scheme,

providing VBUS for external device, assuming i.MX6 OTG is in USB host mode. 

OCC and OCA fields of USB PORTSC1 register are affected by USB_OTG_OC signal

state.

0 Kudos
Reply
2,818 Views
angelo_d
Senior Contributor I

Hi,

i am interested in this.

Why for example sabrelite is not setting this pin (KEY_COL4) as GPIO ? Is it not necessary ?

0 Kudos
Reply