Hi,
I have a custom hardware based on imx6qsabresd. I'm using ltib's u-boot (2009.08).
Is there any reference code for enabling HDMI for splash screen?
Any inputs will be on help?
- Pj
This will be availabe in the upcoming U-boot 2013.10.
If you want to test it now you could use the u-boot-imx tree at: http://git.denx.de/?p=u-boot/u-boot-imx.git;a=summary
Hello Fabio,
Thanks for inputs. Yes, a working reference code will be helpful.
I guess these updates will not be provided to u-boot-2009.08 .. ?
-Pj
No updates for 2009.08.
Please use the latest U-boot from
git://git.denx.de/u-boot.git |
and you will be able to use HDMI on mx6qsabresd.
Here is the patch that adds support for HDMI splashscreen:
Regards,
Fabio Estevam
Hello Fabio,
Thanks a lot for the update and thanks specifically for the link to the patch!!
It will be helpful. I'm using a third part board so kind of stuck to the u-boot 2009.08. When I will start the HDMI task next time, I will try to port (either my setup to latest uboot or HDMI code to my u-boot).
Regards,
Prasant