HI,
i have a usbdm and i want programming a MC9RSKA1. My software is ok, but the flash programming is in trouble. All the time show this message when i will programming the uC.
"programming of the target flash Failed: Reason: BDM is busy"
I using the usbdm flash programmer, version 4.10.5 and my hardware is USBDM-(JMxxCLD).
How fix this problem?
Now the problem that shows is "Target BKGD pin timeout"
Hi Felipe,
I tried out a USBDM_JM60 V1.6 board with a MC9RS08KA1 and it programmed and verified fine with USBDM 4.10.5 and after updating the firmware.
Have you used the programmer on any other chips to confirm if it operates at all?
Could you check the following:
You can also try the tips under testing on this page:
That's about all I can suggest at the moment.
bye
I need to forcing the watchdog reset, do not know why, but it works just as well.
Hi Felipe,
I'm sorry but I don't understand what you mean by "I need to forcing the watchdog reset". Are you talking about the program that you are writing to the Flash or is this something to do with the programmer?
The programmer attempts to disable the COP as part of the chip initialisation. It may have problems connecting if the target already has invalid code that causes a COP or illegal instruction error but it usually copes well.
bye