Hi:
When I do a "build all" with CW 10.4, the progress meter stops ant 7% and stays there for several minutes. If I cancel that build and immediately start another build, it might finish in a few seconds. Sometimes it stalls again, and needs to be restarted twice.
I removed and reinstalled CW 10.4, but nothing changed. My guess is that there is something corrupt in the workspace. Has anybody else had a problem like this?
Thanks,
Michael
Solved! Go to Solution.
hi Michael,
it seems that there are some problems with your workspace configuration.
removing the .metadata folder in the workspace and then re-start CW might help.
if the problem still remains, then, could you please upload your project and a screen-shot for further investiagation?
Hi Michael,
It would be helpful to know what processor/toolchain you are using, I'm assuming Kinetis with gcc?
And no, I have not seen this, but here are some ideas to try out or to check:
I hope this helps.
We tried all of the suggestions here and still get the same issue. If we cancel, sometimes we get the build to go through in several seconds and sometimes it just goes to the next c file in the list. The detailed progress is that it is building a file in the workspace.
This cost us tons of time in 10.2 as well and it appears not fixed.
In windows the process that locks up is mingw32-make.exe. The same one that locked up the same way in 10.2. Kill the process or cancel and rerun it and the next 3 or 4 times it will likely get through the entire make.
We have the same problems described here with the start and stopping. When we went to 10.4 we started with a clean workspace so I dont see how deleting the meta data folder will help but I guess we can try.
Hi Erich:
Thanks for the reply.
The mcu is 9s08qe32. I don't think I did anything to change the tool chain. I was hoping the something like your "cwide -clean" would help, but no change.
I also get a variety of odd behaviour, Such as:
cw says null pointers causing problems
cw unable to find $(ProjDirFile)
message "errors in project, continue launch?" when the Console tab and Problems tab don't show any error I can find.
i get warning about "file system out of sync" when I export a project.
the Progress pane shows one task "build before launch - building dct.abs"
the debugger complains about "no application". The Main tab of the debugger configuration dialog shows the correct file.
A stalled build will stay stalled for hours. If I cancel a build and start another build it will either finish in seconds or stall again. I don't think I have ever needed more than two restarts.
hi Michael,
it seems that there are some problems with your workspace configuration.
removing the .metadata folder in the workspace and then re-start CW might help.
if the problem still remains, then, could you please upload your project and a screen-shot for further investiagation?
Haven't had a "stall" since deleteing the .metadata.
Thanks
Michael