Hi ,
I'm using BSP 4.0.0 to build rootfs for imx6q. I have enabled the option to build rootfs.ext2:
I'm getting the following error:
Filesystem stats, including padding:
Total size = 752424k
Total number of files = 7864
Your ramdisk exceeds the old default size of 4096k, you may need to
set the command line argument for ramdisk_size in your bootloader
allowing 10% free this gives 827666k . For instance, for u-boot:
setenv bootargs root=/dev/ram rw ramdisk_size=827666
creating an ext2 compressed filesystem image: rootfs.ext2.gz
genext2fs: Running in LTIB backwards compatibility mode: -i -> -N
genext2fs: couldn't allocate a block (no free space)
Died at ./ltib line 603, <> line 664.
traceback:
main:603
Started: Thu May 23 13:54:49 2013
Ended: Thu May 23 13:56:09 2013
Elapsed: 80 seconds
Build Failed
Exiting on error or interrupt
Solved! Go to Solution.
It looks like ltib/bin/Ltibutils.pm is not calculating the rootfs size correctly!
I changed this line:
genext2fs -U -b $blocks -i $inodes -D $dev_tab -d $stage $tdir/rootfs.ext2
To
genext2fs -U -b $fs_size_p10 -i $inodes -D $dev_tab -d $stage $tdir/rootfs.ext2
It's not the best fix but this works for now.
Ok I am getting the same error as above using L3.0.35_4.0.0_130424_source.tar.gz Linux BSP for imx6Q on SabreSD platform. The rootfs built fine with all the default options initially and ran fine on my system. Then I tinkered with some kernel settings to enable support for USB Modem. After that ltib tried to rebuild the rootfs.ext2.gz and I got this error:
Processing deployment operations
==================================
making filesystem image file
staging directory is /mnt/veriton/umar/imx6/ltib/rootfs.tmp
sh: line 1: 12305 Broken pipe find . -perm -444 ! -type b ! -type c -print0
12306 Segmentation fault (core dumped) | cpio -p0d --quiet /mnt/veriton/umar/imx6/ltib/rootfs.tmp
Died at ./ltib line 603, <> line 678.
traceback:
main:603
Started: Wed May 29 16:24:20 2013
Ended: Wed May 29 16:24:27 2013
Elapsed: 7 seconds
Build Failed
Exiting on error or interrupt
Please advise.
It looks like ltib/bin/Ltibutils.pm is not calculating the rootfs size correctly!
I changed this line:
genext2fs -U -b $blocks -i $inodes -D $dev_tab -d $stage $tdir/rootfs.ext2
To
genext2fs -U -b $fs_size_p10 -i $inodes -D $dev_tab -d $stage $tdir/rootfs.ext2
It's not the best fix but this works for now.
Thanks Tarek.
I didn't try out your solution because I did a clean re-build and the issue seems to have disappeared.