Hello,
Could someone help me with the LTIB for iMX28?
I'm using Ubuntu12.04 and I'm getting some error with rpm-fs.
Log:
"
Processing platform: host support
===================================
Processing: rpm-fs
====================
ERROR: /tmp/rpm-gbrennon/RPMS/x86_64/rpm-fs-4.0.4-1.x86_64.rpm
would clobber '/reescale/ltib'
traceback:
main::check_host_clobber:2676
main::build_rpm:906
main::f_buildrpms:980
main::check_rpm_setup:2407
main::host_checks:1423
main:542
Started: Tue Jan 8 15:26:08 2013
Ended: Tue Jan 8 15:26:09 2013
Elapsed: 1 seconds
"
As Otavio pointed out I would recommend you take a look at Yocto. I was able to get the Yocto build system running on Ubuntu 12.04 without issue. Just follow the Yocto Quick Start guide. The meta-fsl-arm build for the MX53 built without issue and booted right up. I plan on testing the MX28 soon as well.
Good luck,
Jeff
Yes; it is very easy to build ready to use images and it is also very flexible.
For iMX28 we have ready to use linux-3.7 with most hw supported so it might be good to test as well.
Hello Gláuber ,
I would often find that LTIB would fail because I needed to install a required package. After installing the missing package LTIB would fail as you saw because it refused to overwrite a file it had created on the previous attempt. Just delete the entire LTIB created file structure and start from scratch.
Regards,
Mike
Hi,
Following link will be useful to you.
https://community.freescale.com/docs/DOC-1442
Thanks,
Saurabh
Hello gláuberazevedo,
I am not a LTIB user but a Yocto developer and I'd like to ask you to give a try in Yocto. It provides full support for newer host distributions and has a very updated software stack. We have add support for mx28evk and it should be easy for you to give it a try.
You can check more at Freescale/fsl-community-bsp-platform · GitHub as it has a small documentation how to start. If you want to learn more about Yocto itself you can learn more at https://www.yoctoproject.org/documentation/current.
Regards,