Hi,
I installed the basic rootfs from the"L3.0.35_12.09.01_GA_images_MX6Q" packages. I am trying to configure a static ip permanently and have n idea how to do this. In the meantime I am configuring the ip with 'ifconfig' every time I switch on the card.
Thanks,
David.
Solved! Go to Solution.
You can pass the IP you want in the kernel command line (from the bootloader) like this:
ip=192.168.1.102:192.168.1.101
,where
192.168.1.101: is the serverip IP address
192.168.1.102: is the target (mx6 board) IP address
Regards,
Fabio Estevam
Thanks!
You can pass the IP you want in the kernel command line (from the bootloader) like this:
ip=192.168.1.102:192.168.1.101
,where
192.168.1.101: is the serverip IP address
192.168.1.102: is the target (mx6 board) IP address
Regards,
Fabio Estevam