RTS on USB CDC device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTS on USB CDC device

Jump to solution
1,919 Views
Teckna
Contributor V

Hi everyone,

My device acts as a USB CDC device, my system is CW 10.2 and MQX 3.8.1; the communication channel needs a hardware flow control, I need to simulate the RTS signal to the host (and to get the simulated host CTS signal, of course!).

How can I implement this mechanism?

Is a notification event or an application event?

Many thanks

Teckna

Labels (1)
Tags (5)
0 Kudos
Reply
1 Solution
818 Views
DavidS
NXP Employee
NXP Employee

Hi Teckna,

I'm not USB expert at all (can spell it and plug mouse/keyboard/USB_Stick in).

Have you looked at the MQX example and its _README.pdf?

C:\Freescale\Freescale MQX 3.8b1\usb\device\examples\cdc\virtual_com

Page 6 has:

The USB_Notif_Callback, which is part of the callbacks initialized by

TestApp_Init is a callback function that the CDC class code uses to

signal to the user that a CDC event has happened. The four conditions

it handles are DTE activation and deactivation (for compatibility with

hardware flow control as in traditional UARTs), data received, and send

complete. The DTE conditions set and clear the start_transactions

variable which is tested in receive and send condition checks to make

sure data can be sent or received.

Hope this helps.

Regards,

David

View solution in original post

0 Kudos
Reply
2 Replies
819 Views
DavidS
NXP Employee
NXP Employee

Hi Teckna,

I'm not USB expert at all (can spell it and plug mouse/keyboard/USB_Stick in).

Have you looked at the MQX example and its _README.pdf?

C:\Freescale\Freescale MQX 3.8b1\usb\device\examples\cdc\virtual_com

Page 6 has:

The USB_Notif_Callback, which is part of the callbacks initialized by

TestApp_Init is a callback function that the CDC class code uses to

signal to the user that a CDC event has happened. The four conditions

it handles are DTE activation and deactivation (for compatibility with

hardware flow control as in traditional UARTs), data received, and send

complete. The DTE conditions set and clear the start_transactions

variable which is tested in receive and send condition checks to make

sure data can be sent or received.

Hope this helps.

Regards,

David

0 Kudos
Reply
818 Views
richardtseng
Contributor I

In our case:

PC host == DTE

K60 CDC device == DCE

In the MQX USB CDC example, USB_Notif_Callback() shows how K60 DCE can handle CDC activation/deactivation signal from DTE.

How about sending CDC activation/deactivation signal from K60 DCE to DTE ? Is there a USB device API to send activation/deactivation signal ?

Thanks,

Richard

0 Kudos
Reply