I have a KITMMA955XLEVM: Sensor Toolbox for Xtrinsic Smart Sensing Platform, and using CodeWarrior 10.2.
I am trying to create a custom program and load it on to the microcontroller. However, I am unable to connect or even find the microcontroller when attempting to enter debug mode.
I'm running a Bareboard Project with Open Source BDM. The board is connected to the computer through a single USB cable. I am able to use Sensor Toolbox to read the data from the board. The CPU type on the board is MCF51QE64CLH.
I am running on Windows 7 Home Premium 64-bit. I've tried re-installing the drivers from PEMicro.com, but nothing shows up in Device Manager.
Any help or advice would be greatly appreciated. Cheers.