Hi,
Here we are using CHIMEI LQ035NC111 3.45" TFT LCD MODULE(Synchronous LCD Display) with our custom imx25 board with Linux kernel 2.6.31.
I want to know what are the configuration need to be done with Linux kernel source. i did not find any document related to Linux configuration
Please help me to solve.
Thanks in Advance
Regards
Gokul
Hi Gokul,
you can refer to the settings in ldb.c to support the lvds display panel.
static struct fb_videomode ldb_modedb[] = {
{
"LDB-XGA", 60, 1024, 768, 15385,
220, 40,
21, 7,
60, 10,
0,
FB_VMODE_NONINTERLACED,
FB_MODE_IS_DETAILED,},
{
"LDB-1080P60", 60, 1920, 1080, 7692,
100, 40,
30, 3,
10, 2,
0,
FB_VMODE_NONINTERLACED,
FB_MODE_IS_DETAILED,},
};
Regards,
Ray
Where can i change this settings.. which file is responsible for this??
you should change the video mode according to your panel spec.