Hello
Available intrinsic mainly depend on the compiler you are using.
If you are using CodeWarrior for StarCore V2.x.x,
- Take a look at following manual: {Install}\Help\PDF\MW Enterprise C Compiler Manual.pdf.
Chapter "Using the Metrowerks Enterprise C Compiler", section "Language Features"
-> "Intrinsic Functions" contains a list of the intrinsic functions available and what they are doing.
- Also look at {Install}\Release_Notes\StarCore_Notes\Compiler_Notes\undoc_intrinsics.txt.
There are some additional information in there, which did not make it to the Reference manual.
If you are using CodeWarrior for StarCore V 3.x
- Take a look at following manual: {Install}\Help\PDF\SC_StarCore_C_Compiler_Reference.pdf.
Chapter "Using the Freescale StarCore C Compiler", section "Language Features"
-> "Intrinsic Functions" contains a list of the intrinsic functions available and what they are doing.
There are some general recommendation around which intrinsic a StarCore Compiler should support in the "SC100 Application Binary Interface " (MNSC100ABI) manual available on Freescale web page.
Look at "Chapter 3 High-Level Languages Issues".
I hope this helps a bit
CrasyCat