VGA resolution

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VGA resolution

768 Views
DeanHuang
Contributor III

Hi,

I have two question about VGA resolution of iMX53 QSB .

1. According to release_note of iMX53 QSB, VGA device supports 4 resolution:

    1680x1050, 1280x1024, 1024x768, and 800x600

    But, when I set 1680x1050 and 1280x1024 in uboot, they will become 1024x768.

2. Could we change resolution without uboot?

    I means, uboot is not friendly. We should reboot the OS and write command to uboot through UART.

    Have any other ways to set resolution?

    ps: xrandr is not worked...

Labels (1)
0 Kudos
1 Reply

506 Views
KrishnaPavan
Contributor II

Hi,

What file have you changed to set the resolution?

Can you please specify?

0 Kudos