MC13213-SRB and acquisition...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC13213-SRB and acquisition...

936 Views
Ikoria
Contributor I
Hi all.
I'm Iko, from France (sorry for my english ^^)
 
I try to have information from various phone service but i don't find something...
 
I think i'll buy this dev kit (13213-SRN) for my application.
I try to send sensor value with zigbee. My sensor is a Force Sensitive Resistor (FSR: made by INTERLINK), it's like a various resistor.
 
In the comercial document, it's say "...The boards can also bypass the acceleration sensor to develop customized applications."
 
Then i have two questions.
 
First. Can i use this device to develop a card for acquire and send my sensor value? (the 10bit adc is correct for me) 
 
Second: Has i saw in various discuss, Transmittion rate is like "one data pack" by 1ms ?
 
Thancks for all your informations.
Beast regards.
Iko.
Labels (1)
0 Kudos
Reply
1 Reply

417 Views
Ikoria
Contributor I
Hello.
Sorry for the second post.

I have informations....

I can uses the development board 1321X-SRB .
There are analogue input with 3.3V max....

This is not writte anywhere...


See ya....
0 Kudos
Reply