This is a question raised by one customer.
Currently when Mobis use the MFG tool on Laptop with USB3.0 driver, it can't search the USB port on MFG tool. And then MFG tool is down the program on Laptop.
[Answer] The functionality will be implemented in Mfgtool2.0.
The answer of it will be implemented in MfgTool 2.0 is not an acceptable answer since MfgTool 2.0 does not support the i.MX53. How is someone using an i.MX53 with a PC containing all USB 3.0 ports supposed to use the MfgTool?
If anyone will struggle with this problem, the workaround is disable usb 3.0 support in BIOS settings. All USB ports will be visible as 2.0 and MFG tool will work as it should (at least in my case)
Best regards
There is MFG, supporting USB3