Hi all,
I successfully loaded the appropriate files in a 4GB SD card.
However when the board boots from this new SD card it is getting stuck in the black screen with the linux penguin logo in the upper left corner.
The last messages in the debug are:
VFS: Mounted root (ext3 filesystem) on device 179:1.
Freeing init memory: 172K
init started: BusyBox v1.15.0 ()
starting pid 1176, tty '': '/etc/rc.d/rcS'
Mounting /proc and /sys
Starting the hotplug events dispatcher udevd
Synthesizing initial hotplug events
Setting the hostname to freescale
Mounting filesystems
cp: write error: No space left on device
mount: mounting usbfs on /proc/bus/usb failed: No such file or directory
Starting inetd:
starting pid 2207, tty '': '/sbin/getty -L ttymxc0 115200 vt100
arm-none-linux-gnueabi-gcc (4.4.4_09.06.2010) 4.4.4
root filesystem built on Thu, 24 Nov 2011 17:28:13 -0600
Freescale Semiconductor, Inc.
freescale login:
by typing root i can see the root file system and everything but nothing in the VGA screen.
I will appreciate any opinion/solution
Kostas
just with the username:root is ok,
doesn.t want password
What is the default username and password?
What do you mean with complete compilation?
ok
I thought that it will be a complete compilation.
Is there a documentation for that?
Thanks for the reply
Sounds good. What did you expect to see on the screen? :-)
Default build with LTIB will produce only that on the screen. Now it's up to you to configure the system to start some graphical app (X with some window manager, or GNOME mobile or something else)...