I installed LTIB to /opt/freescale using Ubuntu 11.10 and I am getting this error though I know I installed zlib.
i.e. I installed:
zlib1g,
zlib1g-dbg,
zlib1g-dev and
libghc-zlib-dev.
But I am still getting error below when I run:
./ltib -m config
ltib cannot be run because one or more of the host packages needed to run it
are either missing or out of date or not in ltib's standard path. Please
install/upgrade these packages on your host. If you have your own utilities
in non-standard paths, please add an entry into the .ltibrc file for example:
%path_std
/usr/local/bin:/usr/bin:/bin:/usr/bin/X11:/usr/X11R6/bin:/my/own/exes
Package Minimum ver Installed info
------- ----------- ---------------
zlib 0 not installed
Died at ./ltib line 1397.
traceback:
main::host_checks:1397
main:542
Exiting on error or interrupt
When I try to reinstall "zlib1g-dev" it says I already have the newest version.
I am using ltib 9.1.1 ($Revision: 1.445.6.1 $)
Also aptitude search cannot find zlib-devel.
Anything else I am missing?
Thanks,
Ad.
In perl script ltib (in the beginning) find lines
$cf = {
# configuration options
bldbase => $top
...
pre_install_deps => "
glibc 2.2.4
....
zlib 0
and just comment (#) zlib related line.
The other dependencies (say, flex) may be commented in the same manner.
It was a bug in LTIB scripts not having correct binary path.
I had to edit ltib/bin/Ltibutils.pm
See similar post at:
and the LTIB patch at:
http://lists.nongnu.org/archive/html/ltib/2011-07/txtB5I18k25M7.txt
Now I am off to another problem:
"Exiting on error or interrupt
Please see >> /opt/freescale/ltib/host_config.log for details"
Which is:
pmdb: --force-debian: unknown option
Died at ./ltib line 2340.
traceback:
main::setup_rpmdb:2340
main::check_rpm_setup:2403
main::host_checks:1423
main:542
Ad.
--------------------------------