SGF Drivers - are they compatible for MC9S12xDP512 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SGF Drivers - are they compatible for MC9S12xDP512 ?

1,323 Views
lak
Contributor I
Hi,
I am currently using the motorola sps standard SGF drivers (c-array executable format) for erasing/flashing the MC9S12xDP512 part. when I run the NVMInit() function, I get an error code SGF_INFO_DIS_EEPROM which hints me to enable EEPROM through the INITEE register. But,this register does not exist on the MC9S12xDP512 part.  So, how do I get rid of this error? 
Added, I would like to know , if these drivers do support the MC9S12xDP512 or not?
 
with regards,
Lak 
Labels (1)
0 Kudos
Reply
2 Replies

377 Views
Alban
Senior Contributor II
Hello,
 
INITEE is a register of S12 and not S12X family.
You probably use the drivers from S12.
 
Have you downloaded the drivers from the S12XDP512 product page ?
 
Alban.
0 Kudos
Reply

377 Views
lak
Contributor I
Hi,
Yes, you are right. In the sgf manual, it is mentioned for S12 family.
But I downloaded these drivers (Motorola HCS12 HIS Flash Driver v1.0) under the s12xd family section., i.e, directly under the MC9S12XDP512 section.
are there any separate drivers for the s12x family series?. If yes, can you send me the link
 
with regards,
Lak 
0 Kudos
Reply