Hello,
I configured LTIB for IMX53 qucik start board, but I am missing GCC package.
$ which gcc
which: no gcc in (/bin:/sbin:/usr/bin:/usr/sbin:/usr/local/bin)
Other informations....
$ which make
/usr/bin/make
$ uname -a
Linux freescale 2.6.35.3-744-g27fdf7b #6 PREEMPT Fri Sep 9 05:51:11 PDT 2011 arm
v7l GNU/Linux
Please suggest from where to get the gcc package for 2.6.35.3-744-g27fdf7b kernel for IMX53 board.
Thanks.
Swamy
If you are using the Ubuntu, you can run the command "sudo aptitude -y install gcc" to install the gcc.
By the way, it seems you haven't read the LTIB document "ltib_build_host_setup.pdf", please check it for how to prepare the PC condition for LTIB compiling.
Hi,
I think what Mahadeva is referring to is including gcc not in the host but in the target system.
I too have a custom iMX6q board which has Linux ported on it. However when i try to compile any simple c code in my
linux , it says gcc command not found.
Can you tell me how i can include the gcc tool chain in the kernel or is there any cross compiler which i need to install in my compiler.
regards,
nishad