I bought 5 Freescale educational kits for the Lebanese American University. The kits consist each of a PBMCUSLK Project board (AXM-0392 Rev.B) and a child board (APS12XDT512SLK). Codewarrior for HC(S)12 v4.5 Academic Edition (CWX-H12-STDED-CA) is also supplied.
The Project Board comes with the usb-ml-12 USB debugger. in the documentation it is stated that there is a jumper to select the USB communication speed, the board came with the jumper but no plastic connector (black plastic connector to choose which setting i want) to select which setting. I added one myself.
The main problem is that when debugging a code in Codewarrior the communication with the debugger is lost after about 10~20 steps. if i press ignore for the error the debugging continues but skips the step on which the error occurred.
these are the things i tried: -Running the board form the power adapter/ USB Port.
-Trying the two communication speeds using the jumper j301. Codewarrior always shows a delay of 50 for IO_DELAY_COUNT.
-I tired the P&E unsecure_12.exe utility and the communication works fine so as per P&E's conclusion the hardware is fine.
Running the project board is critical for lab operations.