Hi All
im currently Working with MPC 8280 using CODEWARRIOR V8.8 , when ever i tried to connect it with USB tAP im getting a error message like "Failed to correctly configure the JTAG. and sometimes very rarely it gets connected and once JTAG cable is removed it does'nt gets connected for a long time for so many trials like 80 to 100 so on.
Now i need to know what may be the problem, and whether it is a Hardware issue or do i need to change Code warrior settings.
I am attaching a snapshot of that particular error.
Please help me out and Thanks in advance.
I assume that you are using Windows 7, correct? And a P&E Micro USB probe? You may want to go to the P&E Micro web site (www.pemicro.com) to download and install their latest drivers. I would also use the forum search function (the boxes at the upper right) to search for USB problems with Windows 7. There have been several threads on connection issues.
---Tom
Thanks and Yes i am using windows7 and about PE micro usb port i am not using thar probe. I am trying to dump through Freescale USBTAP JTAAG/COP.
Any Freescale USB TAP interface uses P&E Microsystems drivers and hardware. I've got a DEMO9S08 board (right, it's not the same board, but bear with me) that has an integrated USB/BDM port, and an ASIC on the board with a "PE Micro" label manages the USB/BDM communications. I'd try the P&E Micro driver installation and see if it also does a firmware update.
---Tom