Hello,
I have some of the old MCF5485EVA Boards and used CW 5.7 with MQX2.5 (Custom Bundle for mclog54xx) to program them till now. Now I started with CW10.1 (Eclipse) but i cant get started the application on the M5485 Board.
If i use the Bareboard Project example (CodlFire V4e - MCF5485) i does not get any response from the terminal.
If i use my own projects i get problems with the linker and compiler.
Knows someone what i could use to get it running again? Thx!
In other words. How to intergrate MQX 2.5 or any other MQX version into CW10.1 (based of Eclipse)?
Which settings are importened to get a Board programmed.
Is it possible to use CW 10 to program MCF5485EVB?
I would use an older CW but they arnt running with 64bit OS.
Hi,
you might get proper answer in CodeWarrior section. I checked if there's MCF5485 in project wizard for bareboard project. It's there therefore it should be supported although i have not tested it yet.
Regards,
MartinK