MCF547x/548x Board with CW 10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF547x/548x Board with CW 10

519 Views
MCF5485withCW10
Contributor I

Hello,

 

I have some of the old MCF5485EVA Boards and used CW 5.7 with MQX2.5 (Custom Bundle for mclog54xx) to program them till now. Now I started with CW10.1 (Eclipse) but i cant get started the application on the M5485 Board.

 

If i use the Bareboard Project example (CodlFire V4e - MCF5485) i does not get any response from the terminal.

 

If i use my own projects i get problems with the linker and compiler.

 

Knows someone what i could use to get it running again? Thx!

Labels (1)
0 Kudos
3 Replies

299 Views
MCF5485withCW10
Contributor I

In other words. How to intergrate MQX 2.5 or any other MQX version into CW10.1 (based of Eclipse)?

 

Which settings are importened to get a Board programmed.

0 Kudos

299 Views
MCF5485withCW10
Contributor I

Is it possible to use CW 10 to program MCF5485EVB?

I would use an older CW but they arnt running with 64bit OS.

0 Kudos

299 Views
c0170
Senior Contributor III

Hi,

 

you might get proper answer in CodeWarrior section. I checked if there's MCF5485 in project wizard for bareboard project. It's there therefore it should be supported although i have not tested it yet.

 

Regards,

MartinK

0 Kudos